1. Setting up the Measurement System

The following figure shows the instrument connection of DPD measurement.

In the system connection diagram above, the dark blue lines are for RF connection; the light blue lines are for reference and trigger connection; the black lines are for instrument control connection with LAN or GPIB.

Instrument Requirements

The table shows the requirement for the instruments used in DPD measurement. For details about the options required for each instrument model, refer to System Requirements.

Instrument Type Instrument Model Supported
RF Signal Generator

N5182B MXG

N5172B EXG

Signal Analyzer

N9010A EXA

N9020A MXA

N9030A PXA

System Connection

To set up the measurement system, follow the steps below:

  1. Connect the PC installed with N7614B Signal Studio with the RF Signal Generator and Signal Analyzer through LAN or GPIB.

  2. Connect the EVENT 1 port on the rear panel of the RF Signal Generator to the Trigger IN 1 port on the rear panel of the Signal Analyzer using a BNC cable. This is to synchronize the RF Signal Generator and Signal Analyzer in time domain.

  3. Connect the 10 MHz OUT port on the rear panel of the RF Signal Generator to the EXT REF IN port on the rear panel of the Signal Analyzer using a BNC cable.

  4. Connect the RF OUTPUT port of the RF Signal Generator to the input of the PA and connect the output of the PA to the RF INPUT port of the Signal Analyzer.